AXIS#.WS.STATE

Description

WS switches different current vectors and records position feedback in order to establish commutation alignment.

AXIS#.WS.STATE 0 = wake and shake successful (DONE).

AXIS#.WS.STATE 1 = wake and shake configured and will be done at next enable (ARMED).

AXIS#.WS.STATE 2 = wake and shake running. (ACTIVE)

AXIS#.WS.STATE 10 = error occurred during wake and shake (ERROR).

AXIS#.WS.STATE 11 = wake and shake not required (IDLE).

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

N/A

Default Value

Only valid before the first enable occurs.

11 - for feedback types that do not require wake and shake

1 - for feedback types that require wake and shake
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
AXIS1.WS.STATE

5013h

03h

Unsigned8

-

-

Read only

No

AXIS2.WS.STATE

5113h

03h

Unsigned8

-

-

Read only

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.WS.STATE

6706

1A32

Unsigned8

Read Only

-

AXIS2.WS.STATE

72242

11A3

Unsigned8

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.WS.STATE

6706

Unsigned8

Read Only

-